I designed the circuit dc-dc step up using the ic LT1308B. I assembled it into the breadboard but it didn't work? or I have to assemble it into the PCB. It will work. Thanks.
LT1308
Production
The LT1308 is a micropower, fixed frequency boost DC/DC converter that operates from an input voltage as low as 1V. Capable of delivering 5V at load current...
Datasheet
LT1308 on Analog.com
I designed the circuit dc-dc step up using the ic LT1308B. I assembled it into the breadboard but it didn't work? or I have to assemble it into the PCB. It will work. Thanks.