Post Go back to editing

LTC3122 - variable output voltage

Thread Summary

The user inquires about using the LTC3122 boost converter with a variable output voltage between 5 and 12V, driven by a Maxim MAX5419 digital potentiometer in the R2 feedback position. The final answer confirms that this setup is feasible, with the recommendation to disable the device by pulling the SD pin low during potentiometer adjustments.
AI Generated Content

I would like to use the LTC3122 boost converter in an application where I need a variable voltage level between 5 and 12V.  The input voltage will be between 1.8V and 4.2V.  I was thinking of placing a Maxim MAX5419 digital potentiometer in the R2 position of the feedback network (FB pin to ground).  Do you see any issues with this setup?  I plan to disable the device by pulling SD low during the time when the potentiometer will be adjusted.

Thanks for your help -