Post Go back to editing

ADM7172

Hello!

I need to power five VCO chips,which input voltage is 3.3V and input current is 200mA. I want to use ADM7172ACPZ-3.3-R7 to power that, and the output current of ADM7172 is 2A.

Because of the VCO is Temperature-sensitive, in order to reduce the temperature of power chip, I consider use two ADM7172 to power five VCO chips. One power three VCO chips, and the other power two VCO chips.

The problem is below,

In order to make the supply voltage of these five VCO completely equal,can I connect the two ADM7172 output voltage together, and then power these five VCO?

thanks!!!

Parents Reply Children
No Data