Issue Related to switching of FET in Programmable Current Source

Hi,

I am John working as embedded hardware engineer in Qmax Systems USA.

I am using programmable Current Source (Part : LT3741EUF-1#PBF ) for getting a current output of 20A for battery charging application. I used the typical application circuit of "20A Super Capacitor Charger with 5V Regulated Output" in the datasheet (i have a modification in feedback resistor, so as to get a output voltage of 2.72 V ). The bottom FET is not switching . Plz help me to troubleshoot the issue.

Regards ,

John LT3741EUF-1#PBF.pdf

Parents
  • +1
    •  Analog Employees 
    on Jan 29, 2019 11:50 PM

    I took a close look at your schematic.  It is best to bypass the power VIN rail with 100uF of CERAMIC capacitance.  Your schematic has a 100uF electrolytic on the power VIN rail.  Even with high-performance electrolytic capacitors like hybrid polymers, a few ceramic capacitors in addition are a good idea to bypass the power VIN rail.  Make sure the electrolytic capacitors on your output rail are high-performance (low ESR) as well.  Also, the inductor on your schematic is undersized for 20A out.  The LT3741-1 will not switch at all if the LT3741-1 thinks FB or SENSE+, SENSE- are in regulation.  The bottom FET probably stays off at start up until SS ramps up.  At higher output currents where DCM is not possible, the bottom FET should switch.

Reply
  • +1
    •  Analog Employees 
    on Jan 29, 2019 11:50 PM

    I took a close look at your schematic.  It is best to bypass the power VIN rail with 100uF of CERAMIC capacitance.  Your schematic has a 100uF electrolytic on the power VIN rail.  Even with high-performance electrolytic capacitors like hybrid polymers, a few ceramic capacitors in addition are a good idea to bypass the power VIN rail.  Make sure the electrolytic capacitors on your output rail are high-performance (low ESR) as well.  Also, the inductor on your schematic is undersized for 20A out.  The LT3741-1 will not switch at all if the LT3741-1 thinks FB or SENSE+, SENSE- are in regulation.  The bottom FET probably stays off at start up until SS ramps up.  At higher output currents where DCM is not possible, the bottom FET should switch.

Children
No Data