LT8471
Recommended for New Designs
The LT8471 is a dual PWM DC/DC converter containing two internal 2A, 50V switches and an additional 500mA switch to facilitate step-down and inverting...
Datasheet
LT8471 on Analog.com
LT3514
Production
The LT3514 consists of three buck regulators (2A, 1A, 1A output current). The device has a wide operating input range of 3.2V to 36V. An on-chip boost...
Datasheet
LT3514 on Analog.com
Hi
We are planning to use LT8471 chip for providing VCC to opamp i.e. operating at 12V and -12V
Is this IC is able to provide 12V,2A and -12V ,250mA or 500mA.
We are going to use this 12V,2A into designing 5V/1A 3.3 V/2A and 1.8V/1A using LT3514 chip.
We are using 24V/2A adaptor to provide input to LT8471 chip.
Can you please help in this.
If any application note is available please provide.