Post Go back to editing

LT3652 transition from shutdown to charge

Hello,

We have two boards, the Sunny Buddy, LT3652 based, and the DC1621 with the LTM8062. More o less similars. In both cases, it occurs that they present an intermediate state between low current shutdown mode and charging mode. In this transition state, the circuit sinks a current of several milliamps draining the battery. Depending on the light conditions, this state can be prolonged over time. Are we doing something wrong or should we manage the SHDN # pin in a different way of a simple voltage divider? Perhaps with a comparator?

Best Regards

  • Hello,

    Do you mean when the part is not in SHDN and not charging? Any battery charger will pull some current from the battery when not charging if VIN is not present, just to stay alive. Several mA seems high, though. I can't speak for the Sunny Buddy design as it is done by a third-party manufacturer, but the LT3652 has a quirk where it allows some leakage back to VIN through the BAT pin (part of the reason for the blocking diode on the input). If you have significant leakage paths to GND from VIN (setting resistors, etc), that will increase the drain on the battery. This should still all be very little leakage current, though.

    I can't speak for the LTM8062 but perhaps someone else can.

    Also, consider LTC4162 for cheap, monolithic, battery charger operation with a very low leakage current and a lot of other great features (you can use it standalone as well, despite the digital interface).

    Regards,

    Zack