Post Go back to editing

LTC3775 FAIL

Hi,
I'm using the LTC3775 and I'm a little confusing because the exposed pad is connected to PGND. In the past I have used other controllers, like LTC3851 and LTC7149, and I have always seen the exposed pad connected to the signal ground. Why in the LTC3775 there is this solution? I'm asking because I had some failure with damage in the LTC3775 where, when I rise the load, after few seconds, the LTC3775 shut down. When I tried to restart the circuit I found that the SW pin is in short with the SGND or the BG pin is in short with the PGND. Is there someone that can help?

Parents Reply Children
No Data