Post Go back to editing

Synchronizing multiple uModules

I am using the following uModules in my design: two of LTM4678, LTM4677, LTM4676, and an LTM4686.  I plan to synchronize all at 500KHz and spread the phases to relieve the instantaneous current requirements on their common 12V input source.  I plan to use one SYNC as output from one LTM4678 to drive the other SYNC inputs (SYNC output disabled on these). SYNC has  4.7K pullup, and all SHARE_CLK pins are tied together and SHARE_CLK has a 10K pullup.   I this the correct way to do this?  I have read the datasheets a few times, and looked at the eval board design.  I need this to work first time (like who doesn't)!

Thank You for any insight you can provide.

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.