Post Go back to editing

LTC3780+AD5174

Thread Summary

The user is experiencing issues with the output voltage not changing when using the AD5174 digital rheostat to control the LTC3780. The solution involves setting the AD5174 resistance value before powering on the LTC3780, as changing the resistance while the LTC3780 is running does not affect the output voltage. A pullup resistor on the SDO line of the AD5174 is also suggested to ensure proper communication.
AI Generated Content

Hello! I make a charger for assembling 6S using LTC3780 and MCU STM32. To change the output voltage of the LTC3780, I use a digital rheostat AD5174. Part of the circuit with LTC3780 and AD5174 attached. In this form, this circuit does not work: the output voltage does not change. Individually, the digital rheostat is controlled (checked by deleting it from the circuit), the LTC3780 itself works as it should (connected a mechanical potentiometer instead of the AD5174 and the calculated value of the output voltage corresponds to the actually measured). Why don't LTC3780 and AD5174 work together?

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.