KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
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
LTC3607
Production
The LTC3607 is a 15V dual 600mA monolithic synchronous step-down regulator which has only 55μA quiescent current. Intended for a variety of applications...
Datasheet
LTC3607 on Analog.com
I am using the LTC3607 Dual 600mA DC/DC regulator. The LTC3607 is working in my design without any issues supplying +4, and +5V. My question is: when I remove the input power (+8V) the output will shut off after approximately 400uS. Is there any way to decrease the shut off time? I did try using the Enable pin, it also takes approximately 400uS.
LTC3607 will stop switching soon (usually within 1us) once RUN voltage goes low. Then the decay time of the output voltage depends on the output capacitance and the load resistance. To decrease the decay time, you can reduce the output capacitance (please evaluate the stability) or increase the load current.