Post Go back to editing

register value for LTC4266 90W mode

Dear ADI-er.

Why the vlaue is different two cases(Code & Picture)?

Plz help me.

PortHandler.c of SemiAutoHost_LTPoE++_4266_v1p7p1_Apr_09_2012.zip

   switch(class) {
      case CLASS_1:   cut = 0xC6; lim = 0x80; break; // CUT=112mA; LIM=425mA
      case CLASS_2:   cut = 0xCB; lim = 0x80; break; // CUT=206mA; LIM=425mA
      case CLASS_4:   cut = 0xE2; lim = 0xC0; break; // CUT=638mA; LIM=850mA
      case CLASS_35W: cut = 0x96; lim = 0xE0; break; // CUT=825mA; LIM=1275mA
      case CLASS_45W: cut = 0x9F; lim = 0xE0; break; // CUT=1163mA;LIM=1275mA
      case CLASS_70W: cut = 0xAC; lim = 0x68; break; // CUT=1650mA;LIM=1913mA
      case CLASS_90W: cut = 0xBE; lim = 0x78; break; // CUT=2325mA;LIM=2338mA
      default:        cut = 0xD4; lim = 0x80; break; // CUT=375mA; LIM=425mA
   }



correct the sentence
[edited by: elcielo at 9:43 AM (GMT 0) on 11 Dec 2018]