Post Go back to editing

LTC3569 EN Pins

I am designing a circuit with the LTC3569.

I want to operate it as 3 independent buck converters (1.2A, 0.6A, 0.6A).  I do not have any digital means of controlling the EN pins to set the reference voltages for each converter -- and am fine using the default value.

Questions:

1. Is the default value 0.8V?

2. What should I tie the EN pins to for the behavior described above?  I do NOT want slaved outputs  (which happen to be the only examples in the data sheet).  If I can't pull them to SVin, I assume tying them to SGND would disable that particular buck.  Is there some intermediate voltage?  Should they be floating?  Can I sequence them?  Meaning, tie EN1 to SVin, then EN2 to OUT1, and EN3 to OUT2?

Thanks in advance for your help!

Top Replies

Parents
  • Tried modeling the device by tying the EN pins high (to SVIN), but nothing happens. Am I doing something wrong in the simulation, or is my design wrong?  Does the model allow the pins to be tied high?

    Note -- I tried running with the command .tran 1.2m startup, but the simulation speed was prohibitively slow -- averaged 44ns/s of simulation time

Reply
  • Tried modeling the device by tying the EN pins high (to SVIN), but nothing happens. Am I doing something wrong in the simulation, or is my design wrong?  Does the model allow the pins to be tied high?

    Note -- I tried running with the command .tran 1.2m startup, but the simulation speed was prohibitively slow -- averaged 44ns/s of simulation time

Children
No Data