Post Go back to editing

ADP2118 Current Mode Output

Hello

Since ADP2118 has current mode output, I assume that it is possible to connect two or more of these converters in parallel to increase the current output. I want current output of 6A whereas ADP2118 can support 3A continuous current.

But in the datasheet (or elsewhere) I didn't notice any reference to the possibility of parallel connection of two converters. Is there an application note or reference circuit that I can use?

Regards

Atin

Parents Reply Children
No Data