Hello,
I am interested in using LTM4644 power module.
But I do not understand: is it possible to parallel two of them
to get 8 phase 32A power source for FPGA core supply ?
Datasheet states that "The phase of CLKOUT with respect to
CLKIN is set to 180 deg" so I can't connect CLKOUT of IC1 to CLKIN of IC2.
As I understand, the possible solution could be to use mcu or small fpga with two pwm or timer
each outputs 1 MHz square wave clock shifted 45 degrees between rising edges
(or 125 ns for T=1000 ns)
Could you suggest other solution ?
Best regards,
Igor Petrov,
FPGA Engeneer