ADM1270 maximum ratings are listed below:
at UV, OV and FLB pin are limited to 6V, But if I look at the demo board schematic, when the input voltage is 60V, the UV pin is 6.9V.
Is this condition allowed?
Are there internal clamping diodes on pins?
If yes to which voltage are they referred?
thanks
Fabrizio Erario