LTC-4000 Demo Board Dc1721a-a1

Hi, i'm going to buy the demo board Dc1721a-a1, but before buying I would like to simulate the circuit on LtSpice. Is there already a spice model of the demonstration board?
Also I would like to simulate the various operating states (trickle charge, etc.), can you tell me which battery model to insert and which values ​​to assign to the components of the battery?

Thank you in advance

Parents
  • 0
    •  Analog Employees 
    on Nov 2, 2018 12:16 PM

    Hello, I am not aware of a model with the demo board DC1721a-a. The only simulation model that I am aware of is the LT3845A/LTC4000, which is used on the LTC4000 macromodels test fixture. This can be selected using the select compontent symbol, select LTC4000, then select the "Open this macromodel's test fixture" button in LTSpice.

    I do not have an answer on what is the best battery model to insert.

Reply
  • 0
    •  Analog Employees 
    on Nov 2, 2018 12:16 PM

    Hello, I am not aware of a model with the demo board DC1721a-a. The only simulation model that I am aware of is the LT3845A/LTC4000, which is used on the LTC4000 macromodels test fixture. This can be selected using the select compontent symbol, select LTC4000, then select the "Open this macromodel's test fixture" button in LTSpice.

    I do not have an answer on what is the best battery model to insert.

Children
No Data