Can two or more LTC3892 work in lnterleaved mode?
多个LTC3892可以交错并联工作吗?
For example, two LTC3892 are given two external clock signal with 90-degree difference. And all four VFB are connected together; all four ITH are connected together; all four TRACK are connected together. Can this system work?
例如,把两个相差90度的时钟信号分别给两个3892,把两个3892一共4个通道的VFB连在一起,ITH连在一起,Track连在一起。这样系统能够工作吗?
Can similar methods be used in other chips to build multiphase interleaved system?
类似的方法可以应用于别的芯片以构成多相交错并联的系统吗?