Hi -
I have a quick question about the LT3965. I've designed the device into an system and it works fine. Right now a 1Mhz clock from an oscillator is driving all the RTCLK pins of all the LT3965s in the system. I'm going to stop using the 1Mhz external clock and instead rely on pull down resistors connected to each RTCLK pin right at the chip to set the PWM clock frequency to around 500Hz. Does any of the PWM or fault detection functionality change if I stop using the external 1Mhz clock?
Thanks,
Larry Welch
EPAM Continuum
Boston, MA