Dear Sir
I use the ADP5071 for 5V to + 9V / 0.5A and -9V / 0.2A
I refer to the datasheet on page 20 for RC1, CC1 and RC2, CC2, which is close to the ADP507x design tool.
I saw EZ reply suggesting to use the ADP507x design tool
But data sheets table 10 and 11 confuse me what is correct?
Any suggest ?
refer datasheet calculation RC1=20.15K, CC1=0.53nF
ADP507x design tool RC1=26.1K, CC1=1nF
Table 10, RC1=1.8K, CC1=47nF