Hi, what is the difference between the ordering codes LTC3419EMS#PBF and LTC3419IMS#PBF?
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
LTC3419
Production
The LTC3419 is a dual, 2.25MHz, constant-frequency, synchronous step-down DC/DC converter in a tiny 3mm × 3mm DFN package. 100% duty cycle provides low...
Datasheet
LTC3419 on Analog.com
Hi, what is the difference between the ordering codes LTC3419EMS#PBF and LTC3419IMS#PBF?
Hi,
It is on page 3 of datasheet:about ambient temperature performance
Note 3: The LTC3419E and LTC3419E-1 are guaranteed to meet specifi ed performance from 0°C to 85°C. Specifi cations over the –40°C to 125°C operating junction temperature range are assured by design, characterization and correlation with statistical process controls. The LTC3419I and LTC3419I-1 are guaranteed to meet specifi ed performance over the full –40°C to 125°C operating junction temperature range.