Post Go back to editing

LT3680 in inverting buck boost configuration

Hello,

I want to use the LT3680 in inverting buck boost topology to generate -15V@0.5A from +5V input voltage.

I simulated the design with LTSpice (attached), and everything looks ok, efficiency is app. 78%.

But according to some application notes, the Vin-to-Vout relationship of an inverting buck boost converter must be smaller that the efficiency. Otherwise the maximum output current will be zero.
Thus, the maximum output current should be 0.14A (and not 0.5A) in my design.

Can anybody please confirm if it is possible to generate Vout = -15V/0.5A from Vin = 5V with the LT3680?

Thanks in advance, Niels

LT3680_5V_IBB_-15V_500mA.zip

  • Ok,

    as nobody has an answer to my question, I repeat it in simple words:

    How can I include the switcher's efficiency into the calculation of the maximum output current of the LT3680 in inverting-buck-boost (IBB) configuration?

    I am looking forward to any answer.

    Regards, Niels

  • Hello Niels,

    The higher the efficiency, the more output current an LT3680 inverting buck-boost circuit can deliver. What you can do is measuring the SW node peak current in your LTSpice simulation, then comparing it against the switch current limit in the datasheet. As long as the peak SW current measurement is less than the min. switch current limit. Your application is fine.

    To make it simpler, the LT3680 is a 3.5A buck regulator. So let's say if your measured peak current is less than 4A, you are good to go.

    Hope this helps.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.