Post Go back to editing

ADP2360 as dc-dc converter for loop-powered system

Hi 

I'm designing a board which will be powered from loop-powered system with  24v/3.2mA input.

I want to convert it to 3.3V/12mA output.

So i want to use adp2360 as dc-dc converter but the problem is in LTSpice the minimum input current from supply is 50mA , which can be maximized with Rith.

I want to know if these type of dc-dc converter can be use for loop-powered application , and if not , is there any suggestion?

Thanks

Best Regard