Hello,
Can spread spectrum clock be applied to SYNC pin?
PLL_Unlock status can be seen on the LTpower Play and I like to confirm spread spectrum clock can be used as external clock source.
Best regards,
Hello,
Can spread spectrum clock be applied to SYNC pin?
PLL_Unlock status can be seen on the LTpower Play and I like to confirm spread spectrum clock can be used as external clock source.
Best regards,
From the LTM4676A operation point of view, it can track to 1-2kHz rate change. In your application, what’s the switching frequency and the modulation rate? If the modulation rate is higher than 1-2 kHz so that the LTM4676A couldn’t track it. That's why you see the PLL fault.
Switching frequency is 600kHz and generated by LTC6909.
This 600kHz +/-10% with 9.3kHz modulation rate clock are supplied to LTM4676A.
It seems LTM4676A will not be able to track higher modulation rate clock.
Thank you for your help.