Qestions about ADP5091

Hi,

The data sheet recommeds a 22uH inductance for the boost regulator.

Could you let me know the calculation formula for the inductor ?

 

The data sheet page 1 mentions that ADP5091 can cover up to 600mW input power.

On the other hand, the input peak current of the boost converter is 200mA typ, which means

the input average currernt is roughly 100mA. The input voltage is 3.3V max, then the input power

is 3.3V * 100mA = 330mW. How come the ADP5091 can cover 600mW input power?

 

Are there any difference in ADP5091 performance (starting up, charging to a battery sequence, and so on)

regarding with MPPT and without MTPPT?