Post Go back to editing

LTC4446: Can I use this driver to drive two electrodes?

I am planning to use two PWM signals at 1 MHz and 30% duty cycle as inputs to the BINP and TINP inputs of the LTC4446. Ultimately I would like to output a PWM signal at 1MHz and has a 30% duty cycle, and should have a peak to peak voltage of 0-80V. The output also needs to connect to an electrode with some intrinsic capacitance.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.