is there any model for the ADP1708 LDO IC??
ADP1708
Production
The ADP1706/ADP1707/ADP1708 are CMOS, low dropout linear regulators that operate from 2.5 V to 5.5 V and provide up to 1 A of output current. Using an...
Datasheet
ADP1708 on Analog.com
is there any model for the ADP1708 LDO IC??
Hi,
ADP1708 LTSpice model is not yet available. It will be available soon.
Regards,
Errgy
Where is the model, today is May 09, 2020
Where is the model, today is May 09, 2020
Hi wjy,
Apology for this extreme delay. Unfortunately, this part has never made it to top list. I have raise this concern and we will find a way to get LTspice models to many of our parts. The best way for now is to have a demo board if you want to test critical items like PSRR, noise, load transient. If you need urgently, you can also request data through a local ADI sales or FAE.