Post Go back to editing

ADP1761 variable output voltage

I would like to use the ADP1761 in a low noise application, where the output voltage can range from 0.6 to 1.0 volts (900mA maximum).

The control of this should be via some bus such as I2C / SPI.

Are you able to recommend a suitable controlled resistor or some other way to adjust the ADP1761 output?

Thanks

David

Parents Reply Children
No Data