LTM8074
Recommended for New Designs
The LTM8074 is a 40VIN, 1.2A continuous, 1.75A peak, step-down µModule® (power module) regulator. The Silent Switcher architecture minimizes EMI while...
Datasheet
LTM8074 on Analog.com
Dear ADI colleagues,
My customer use LTM8074 to generate -8V output voltage and it is ok.But when the customer want to shutdown the output of LTM8074 by connect RUN pin to GND,it cannot work.-8V output still exist on the output of LTM8074.I attach the schematic as follows,and the green components in the schematic are not mounted.
please help check when output negative voltage,if it's possible to use RUN pin(connect to <0.9V) to shutdown the LTM8074.
with best regards&thank
Heng
Hi Heng,
Please refer to the article linked below for the proper connection for run pin for this case