Hi,
for the LTC3290 is it possible to have the following configuration?
- Vin between 10 and 14 V
- Vaux of 5 V
- Vout of 12 V
This in the standard boost charge pump, with:
- Vset grounded
- R1=44.2K
- R2=486K
The rule of
Vin + Vaux ≥ Vout + Rol * Iout
would be satisfied (Iout<50mA), but I don't understand if there are some other constraints to be respected.
Thank you in advance.
Clemente