Post Go back to editing

LTC3290 Fixed output voltage inside the input voltage variation range

Category: Datasheet/Specs
Product Number: LTC3290

Hi,
for the LTC3290 is it possible to have the following configuration?

  • Vin between 10 and 14 V
  • Vaux of 5 V
  • Vout of 12 V

This in the standard boost charge pump, with:

  • Vset grounded
  • R1=44.2K
  • R2=486K

The rule of

Vin + Vaux ≥ Vout + Rol * Iout

would be satisfied (Iout<50mA), but I don't understand if there are some other constraints to be respected.

Thank you in advance.

Clemente