Hi. I have problems with LT3763.
As a DCDC-converter with current limitation, this IC should load large capacities (10mF) up to max.12V.
After switching on the power supply, the IC gets very hot and breaks. Short circuit between Pin26 (SW) and GND.
This also happens without a load at the output.
Supply voltage: 48VDC, Output voltage: 12V, Max output current: 2.77A.
The IC is switched on via an MCU
I'v checked all but I have no idea what is wrong.