LT8650S is an external BST capacitor required?

Hello.

Does the LT8650S require an external boost capacitor?   The datasheet pin description says:

"BST1 (Pin 24): This pin is used to provide a drive voltage, higher than the input voltage, to the top side power switch of channel 1. Place a 0.1μF boost capacitor as close as possible to the IC."

But the evaluation board and application examples do not have  BST capacitor, as they are integrated inside the device itself.

Please could you let me know if I need an external BST capacitor.

Thanks.



Update title
[edited by: daedalus at 12:54 PM (GMT 0) on 27 Feb 2020]