Post Go back to editing

LT 3033 malfunctioning

Hello,

I am trying to test the IC : LT 3033. It has a linear regulator with a internal reference voltage of 0.2V. I had set feedback resistors of 150K and 11k to expect an output of 2.9V approx. However I am getting an output voltage of 0.48V at a supply of 4.5V. Also the output voltage is increasing with increase in input voltage. I am attaching the datasheet and a zip file of board and schematic files that I have created in Autodesk eagle 9.1.

lt3033.zipPDF

Parents
  • Hello

    What happens in thermal shutdown and overcurrent shutdown of the IC? I have connected an inductive load at the output and when the current increases beyond a certain value the output voltage starts switching between 0 and the set voltage. However since the load is inductive the current should remain constant, with some ripple because the voltage is not constant. But what is being observed is totally different. The current passing through the inductor drops sharply to 0 when the output voltage of the IC becomes 0 (due to shutdown). So I want to know what exactly happens in a thermal shutdown and overcurrent shutdown.

    The first waveform is current through the inductor. The second waveform is the voltage at the output of the IC.

    The output voltage is increased by changing the value of the resistor divider resistors. Input voltage is 4.2V, current is limited to max of 1A, Inductor = 2.6mH, series resistance = 1.2 Ω, input capacitance = 100uf and output capacitance = 100uf

Reply
  • Hello

    What happens in thermal shutdown and overcurrent shutdown of the IC? I have connected an inductive load at the output and when the current increases beyond a certain value the output voltage starts switching between 0 and the set voltage. However since the load is inductive the current should remain constant, with some ripple because the voltage is not constant. But what is being observed is totally different. The current passing through the inductor drops sharply to 0 when the output voltage of the IC becomes 0 (due to shutdown). So I want to know what exactly happens in a thermal shutdown and overcurrent shutdown.

    The first waveform is current through the inductor. The second waveform is the voltage at the output of the IC.

    The output voltage is increased by changing the value of the resistor divider resistors. Input voltage is 4.2V, current is limited to max of 1A, Inductor = 2.6mH, series resistance = 1.2 Ω, input capacitance = 100uf and output capacitance = 100uf

Children