LT8650S.pdfI realized a board with LT8650S. The schematic is here attached.
My idea is to have two different OUTPUTs VH and VL_I from the LT8650S. The max current for VH will be 1.5A and the max current for VL_I will be 0.5A
In this circuit, I can change the two output voltages by set the voltage (0 to 5V) in the points CTRL_VH and CTRL_VL_1 and so the OUTPUT voltage can vary from 23.9V to 3.83V.
My problems is that in the first application the LT8650S was burned.
Could you check the schematic if you see something wrong?
Thank you.