Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • LEO Satcom: Application of RF, Mixed-Signal, & Beamforming ICs
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    • Revolutionizing Flow Cytometry: 20-Bit Precision Signal Chain
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quiz AQQ300 about Divisibility by 6

      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Improving Industrial Functional Safety Compliance with High Performance Supervisory CircuitsPart 5: Sequencers Eliminate Systematic Failures

    This article shifts focus from managing the quantitative metrics of functional safety toward mastering the qualitative yet equally critical challenge:...

EngineerZone
EngineerZone
Battery Management System
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Battery Management System
  • Power Management
Battery Management System
Documents What are the different memory register types of the MAX17201/205/211/215 and how are they related?
  • Q&A
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADBMS6830: FAQ
  • +ADP5061: FAQ
  • +DS2438: FAQ
  • +DS2438Z+: FAQ
  • +DS2704G+: FAQ
  • +DS2711: FAQ
  • +DS2711E+: FAQ
  • +DS2712E+: FAQ
  • +DS2712EVKIT+: FAQ
  • DS2715: FAQ
  • +DS2715BZ+: FAQ
  • DS2740: FAQ
  • +DS2740U: FAQ
  • +DS2745EVKIT+: FAQ
  • +DS2745U+: FAQ
  • +DS2762AE+: FAQ
  • +DS2764AE+025: FAQ
  • DS2775: FAQ
  • +DS2775G+: FAQ
  • +DS2777: FAQ
  • +DS2781AE+/: FAQ
  • +DS2782E+: FAQ
  • DS2784: FAQ
  • +DS2784G+: FAQ
  • +DS2786: FAQ
  • DS2788: FAQ
  • DS2788E+: FAQ
  • +DS2788E+T&R: FAQ
  • +DS2788EVKIT+: FAQ
  • How do I create a model with DS2788
  • MAX14690: FAQ
  • +MAX14690AEVAL#: FAQ
  • +MAX14745AEWX+: FAQ
  • +MAX14745DEWX+: FAQ
  • +MAX14745GEWX+: FAQ
  • +MAX14745MEWX+T: FAQ
  • +MAX14920ECB+: FAQ
  • +MAX14921 EVKIT SOF: FAQ
  • MAX14921: FAQ
  • +MAX14921ECS+: FAQ
  • +MAX1501: FAQ
  • +MAX1555EZK+T: FAQ
  • +MAX16016: FAQ
  • +MAX1667EAP_T1: FAQ
  • +MAX17043G+T: FAQ
  • +MAX17043G+U: FAQ
  • +MAX17043X+: FAQ
  • MAX17048: FAQ
  • MAX17048G+: FAQ
  • +MAX17048G+CHU: FAQ
  • +MAX17049: FAQ
  • +MAX17050X+T10: FAQ
  • MAX17055: FAQ
  • MAX17055AEWL+: FAQ
  • +MAX17055AEWL+_B1: FAQ
  • MAX17055ETB+: FAQ
  • +MAX17055ETB+T: FAQ
  • +MAX17055EWL+T: FAQ
  • +MAX17055GEVKIT: FAQ
  • +MAX17058: FAQ
  • MAX17201: FAQ
  • MAX17201G+: FAQ
  • -MAX17201G+T0E: FAQ
    • Are external ESD diodes compulsory to use in I2C lines of MAX17201/5, MAX17211/15?
    • Can I use a thermistor with +/-3°C accuracy with a ModelGauge m5 fuel gauge?
    • Can MAX17201/MAX17205/MAX17211/MAX17215 internal LDO's be used to supply external circuitry?
    • Can you use the MAX17201 to Fuel Gauge NiMH batteries?
    • Do I need to burn NV memory for a pack side fuel gauge?
    • For MAX17201 family of fuel gauges, how can I determine when the registers are fully initialized?
    • For MAX17201 family of fuel gauges, is there a way to determine when the NV write process has finished?
    • Fuel Gauge for Primary cell measurement
    • How can I improve the first cycle accuracy of a ModelGauge m5 EZ fuel gauge?
    • How can I test different configuration settings on the MAX17201/5 without using an NV write?
    • How do I get the register settings corresponding to a given battery model for MAX17201/11, MAX17205/15?
    • How do I read the battery cell or pack voltage with the MAX17201 fuel gauge?
    • How do I set the nPackCfg value to eliminate the nPackCfg error on the MAX17201 GUI?
    • In MAX17201/5, How to measure offset current value?
    • Is there any guideline to select current sense resistor (Rsense) in MAX17201 fuel gauge design?
    • MAX17201 power up delay
    • MAX17201EVKIT Fail MTP error when writing to NV memory
    • My MAX17201GEVKIT suffers from a decrease in measured capacity to an unusual high degree (up to 100mAh overnight). This seems not to reflect the real capacity decrease - what can be going wrong?
    • The MAX17201GEVKIT does not connect to the GUI without a battery, is this normal?
    • User guides UG6258 and UG6259 show writes to registers 0x062, 0x063 and 0x080. The datasheet does not have any information on these registers. What are they for?
    • What are the differences between battery model INI and configuration INI?
    • What are the different memory register types of the MAX17201/205/211/215 and how are they related?
    • What can cause the reported capacity of the MAX17201 to be inaccurate?
    • What is the difference between ModelGauge and Modelgauge m5 algorithm in Maxim FuelGuage ICs?
    • What register should the customer use to estimate the self-discharge of a battery over a long period of time?
    • When MAX17201 is configured with primary cell, why the current readings are negative?
    • When the MAX17201G is used for 38Ah battery, how should we select the current sensing resistor?
    • Why do the voltage updates in the MAX17201 take longer than 351ms if I have multiple cells?
    • Writing to NV memory in MAX17201
  • MAX17201G+T: FAQ
  • +MAX17201GEVKIT#: FAQ
  • MAX17205: FAQ
  • MAX17205G+: FAQ
  • +MAX17205G+T: FAQ
  • +MAX17205GEVKIT#: FAQ
  • +MAX17211G+: FAQ
  • +MAX17215G+: FAQ
  • +MAX17260 EVALUATION KIT SOFTWARE: FAQ
  • MAX17260BEWL+: FAQ
  • +MAX17260BEWL+_B1: FAQ
  • +MAX17260SETD+: FAQ
  • +MAX17260SEWL+: FAQ
  • +MAX17260XEVKIT#: FAQ
  • +MAX17261GEVKIT#: FAQ
  • MAX17261METD+: FAQ
  • +MAX17261METD+T: FAQ
  • +MAX17261MEWL+: FAQ
  • +MAX17261XEVKIT#: FAQ
  • +MAX17262REWL+: FAQ
  • +MAX17263GEVKIT#: FAQ
  • +MAX17263LETD+: FAQ
  • +MAX17301G+: FAQ
  • +MAX17301GEVKIT#: FAQ
  • +MAX17303G+: FAQ
  • +MAX17303X+T: FAQ
  • +MAX17313G+: FAQ
  • +MAX17320G10+: FAQ
  • +MAX17320G1EVKIT#: FAQ
  • +MAX17320G20+: FAQ
  • +MAX17320X22+: FAQ
  • +MAX17320X2EVKIT#: FAQ
  • MAX1737: FAQ
  • +MAX1737EEI+T: FAQ
  • +MAX17435: FAQ
  • +MAX1757EAI+: FAQ
  • +MAX1758EAI (28-SSOP): FAQ
  • +MAX1758EAI+: FAQ
  • +MAX17703ATG+: FAQ
  • MAX17823BGCB/V+: FAQ
  • +MAX17823BGCB/V+T: FAQ
  • +MAX17841BGUE/V+T: FAQ
  • MAX17843: FAQ
  • MAX17843ACB/V+: FAQ
  • +MAX17843ACB/V+_T1: FAQ
  • +MAX17851EVKIT#: FAQ
  • +MAX17852ACB/V+: FAQ
  • +MAX17852EVKIT#: FAQ
  • +MAX17853ACB/V+: FAQ
  • +MAX17853EVKIT#: FAQ
  • +MAX1870AETJ+: FAQ
  • +MAX1873REEE+: FAQ
  • MAX1873REEE: FAQ
  • +MAX1873TEEE+: FAQ
  • +MAX20094ATI/VY+: FAQ
  • +MAX20094ATIB/VY+: FAQ
  • MAX20303: FAQ
  • MAX20303AEWN+: FAQ
  • +MAX20303AEWN+T: FAQ
  • +MAX20303BEWN+: FAQ
  • +MAX20303EVKIT#: FAQ
  • +MAX20303EWN+: FAQ
  • +MAX20335AEWX+: FAQ
  • +MAX20353: FAQ
  • +MAX20360AEWZ+: FAQ
  • +MAX6361: FAQ
  • MAX6900: FAQ
  • +MAX6900ETTAEQ-T: FAQ
  • +MAX6953EAX+: FAQ
  • +MAX713: FAQ
  • +MAX7452: FAQ
  • +MAX7456EUI+_T1: FAQ
  • MAX77650: FAQ
  • +MAX77650AEWV+: FAQ
  • +MAX77650BEWV+: FAQ
  • +MAX77650CEWV+: FAQ
  • +MAX77651AEWV+: FAQ
  • +MAX77654AENV+: FAQ
  • +MAX77654AENVN+: FAQ
  • +MAX77654BENV+: FAQ
  • +MAX77654_NV+_A1: FAQ
  • +MAX77734AENP+T: FAQ
  • +MAX77734BENP+: FAQ
  • +MAX77818 CHARGER+F: FAQ
  • +MAX77818EVKIT#: FAQ
  • +MAX77818EVSYS#: FAQ
  • MAX77818EWZ+: FAQ
  • +MAX77818EWZ+T: FAQ
  • +MAX77840EVKIT#: FAQ
  • MAX77950: FAQ
  • +MAX77950EVKIT#: FAQ
  • +MAX77950EWW+_B1: FAQ
  • +MAX77960BEFV06+: FAQ
  • MAX77961EFV+: FAQ
  • +MAX77961EFV+T: FAQ
  • +MAX77961EFV06+T: FAQ
  • +MAX77962EWJ+_B1: FAQ
  • +MAX77962EWJ12+: FAQ
  • +MAX77975EFD+: FAQ
  • +MAX77976EFD+: FAQ
  • +MAX8677AETG+: FAQ
  • +MAX8713EVKIT: FAQ
  • +MAX8856ETD+: FAQ
  • +MAX8895VEWA+: FAQ
  • +MAX8903A: FAQ
  • +MAX8934AETI+: FAQ
  • MAX8971: FAQ
  • +MAX8971CEWP+: FAQ
  • +MAX8971EWP+T: FAQ

What are the different memory register types of the MAX17201/205/211/215 and how are they related?

Registers starting with a lowercase 'n' like nTGAIN and nTOFF are located in a space called Non-Volatile Shadow memory. This space is a volatile SRAM value that gets updated to the value of the relevant non-volatile memory data when the part is reset or through a recall command. While the part is powered this space can be modified by I2C as needed and behaves as a typical RAM. 

Registers that don't start with the lowercase 'n' such as TGAIN and TOFF are also SRAM registers that are prepared at startup by values calculated by the firmware. If the firware looks at the shadow nNVCfg registers (non-volatile) and decides to use the nTGAIN and nTOFF values (via the enTGO bit), then TGAIN and TOFF will be prepared with the shadow values. If in this example the enTGO bit is not set, the firmware will look at the values that are saved in the ROM (firmware code) and use those values to setup the TGAIN and TOFF registers. In the case that default ROM values are used, this frees up the nTGAIN and nTOFF registers for use as general purpose non-volatile memory storage. 

 

=============================================================Got this explanation from the BU AE===============================

Tags: KA-05874 non-volatile nonvolatile MAX17211 MAX17201 MAX17215 memory MAX17205 volatile MAX17201G+ Show More