This webinar will introduce remote-controlled edge nodes and how they promise to simplify the automotive network architecture and expedite the integration...
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
      1. Quote of the week: "Knowledge is knowing a tomato is a fruit. Wisdom is not putting it in a fruit salad" - unknown Sources: commons.wikimedia...

    View All

    What's Brewing

      Quiz! Why a Hybrid Approach Works Blog and Test Your Knowledge

      Quiz! Understand ISO 26262 Compliance Test your knowledge with our quick quiz , based on the blog " Safety in Layers: Why a Hybrid Approach Works ...
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
    The Limitation of Heat Dissipation IO-Link is used across many branches of factory automation, and in these applications, areas of the factory floor...

     

    GMSL Debugging: Getting a Lock

    Imagine a scenario where you have a brand-new board design or are excited to try out some evaluation kits only to find out that the two devices can’t talk...
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
Battery Management System
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Battery Management System
  • Power Management
Battery Management System
Documents How does the Burst mode in the MAX14745 work?
  • Q&A
  • FAQs/ Docs
  • Members
  • Tags
  • More
  • Cancel
  • +Documents
  • +ADBMS6830: FAQ
  • +ADP5061: FAQ
  • +DS2438: FAQ
  • +DS2438Z+: FAQ
  • +DS2704G+: FAQ
  • +DS2711: FAQ
  • +DS2711E+: FAQ
  • +DS2712E+: FAQ
  • +DS2712EVKIT+: FAQ
  • DS2715: FAQ
  • +DS2715BZ+: FAQ
  • DS2740: FAQ
  • +DS2740U: FAQ
  • +DS2745EVKIT+: FAQ
  • +DS2745U+: FAQ
  • +DS2762AE+: FAQ
  • +DS2764AE+025: FAQ
  • DS2775: FAQ
  • +DS2775G+: FAQ
  • +DS2777: FAQ
  • +DS2781AE+/: FAQ
  • +DS2782E+: FAQ
  • DS2784: FAQ
  • +DS2784G+: FAQ
  • +DS2786: FAQ
  • DS2788: FAQ
  • DS2788E+: FAQ
  • +DS2788E+T&R: FAQ
  • +DS2788EVKIT+: FAQ
  • How do I create a model with DS2788
  • MAX14690: FAQ
  • +MAX14690AEVAL#: FAQ
  • -MAX14745AEWX+: FAQ
    • For MAX14745, what's the feature for adaptive current limit?
    • How does the Burst mode in the MAX14745 work?
    • How does the switching frequency varies in Burst/PFM mode and how it affects EMI in the MAX14745?
    • Is the switching between PWM/PFM mode strictly a function of the load applied in the MAX14745?
    • MAX14745 does not have a watch dog feature, how to add this function to the PMIC
    • Per MAX14745 datasheet, the part seems only can use 10KΩ for NTC. Can this part use 100KΩ NTC?
    • What's the difference between the MAX14745 and the MAX14690?
  • +MAX14745DEWX+: FAQ
  • +MAX14745GEWX+: FAQ
  • +MAX14745MEWX+T: FAQ
  • +MAX14920ECB+: FAQ
  • +MAX14921 EVKIT SOF: FAQ
  • MAX14921: FAQ
  • +MAX14921ECS+: FAQ
  • +MAX1501: FAQ
  • +MAX1555EZK+T: FAQ
  • +MAX16016: FAQ
  • +MAX1667EAP_T1: FAQ
  • +MAX17043G+T: FAQ
  • +MAX17043G+U: FAQ
  • +MAX17043X+: FAQ
  • MAX17048: FAQ
  • MAX17048G+: FAQ
  • +MAX17048G+CHU: FAQ
  • +MAX17049: FAQ
  • +MAX17050X+T10: FAQ
  • MAX17055: FAQ
  • MAX17055AEWL+: FAQ
  • +MAX17055AEWL+_B1: FAQ
  • MAX17055ETB+: FAQ
  • +MAX17055ETB+T: FAQ
  • +MAX17055EWL+T: FAQ
  • +MAX17055GEVKIT: FAQ
  • +MAX17058: FAQ
  • MAX17201: FAQ
  • MAX17201G+: FAQ
  • +MAX17201G+T0E: FAQ
  • MAX17201G+T: FAQ
  • +MAX17201GEVKIT#: FAQ
  • MAX17205: FAQ
  • MAX17205G+: FAQ
  • +MAX17205G+T: FAQ
  • +MAX17205GEVKIT#: FAQ
  • +MAX17211G+: FAQ
  • +MAX17215G+: FAQ
  • +MAX17260 EVALUATION KIT SOFTWARE: FAQ
  • MAX17260BEWL+: FAQ
  • +MAX17260BEWL+_B1: FAQ
  • +MAX17260SETD+: FAQ
  • +MAX17260SEWL+: FAQ
  • +MAX17260XEVKIT#: FAQ
  • +MAX17261GEVKIT#: FAQ
  • MAX17261METD+: FAQ
  • +MAX17261METD+T: FAQ
  • +MAX17261MEWL+: FAQ
  • +MAX17261XEVKIT#: FAQ
  • +MAX17262REWL+: FAQ
  • +MAX17263GEVKIT#: FAQ
  • +MAX17263LETD+: FAQ
  • +MAX17301G+: FAQ
  • +MAX17301GEVKIT#: FAQ
  • +MAX17303G+: FAQ
  • +MAX17303X+T: FAQ
  • +MAX17313G+: FAQ
  • +MAX17320G10+: FAQ
  • +MAX17320G1EVKIT#: FAQ
  • +MAX17320G20+: FAQ
  • +MAX17320X22+: FAQ
  • +MAX17320X2EVKIT#: FAQ
  • MAX1737: FAQ
  • +MAX1737EEI+T: FAQ
  • +MAX17435: FAQ
  • +MAX1757EAI+: FAQ
  • +MAX1758EAI (28-SSOP): FAQ
  • +MAX1758EAI+: FAQ
  • +MAX17703ATG+: FAQ
  • MAX17823BGCB/V+: FAQ
  • +MAX17823BGCB/V+T: FAQ
  • +MAX17841BGUE/V+T: FAQ
  • MAX17843: FAQ
  • MAX17843ACB/V+: FAQ
  • +MAX17843ACB/V+_T1: FAQ
  • +MAX17851EVKIT#: FAQ
  • +MAX17852ACB/V+: FAQ
  • +MAX17852EVKIT#: FAQ
  • +MAX17853ACB/V+: FAQ
  • +MAX17853EVKIT#: FAQ
  • +MAX1870AETJ+: FAQ
  • +MAX1873REEE+: FAQ
  • MAX1873REEE: FAQ
  • +MAX1873TEEE+: FAQ
  • +MAX20094ATI/VY+: FAQ
  • +MAX20094ATIB/VY+: FAQ
  • MAX20303: FAQ
  • MAX20303AEWN+: FAQ
  • +MAX20303AEWN+T: FAQ
  • +MAX20303BEWN+: FAQ
  • +MAX20303EVKIT#: FAQ
  • +MAX20303EWN+: FAQ
  • +MAX20335AEWX+: FAQ
  • +MAX20353: FAQ
  • +MAX20360AEWZ+: FAQ
  • +MAX6361: FAQ
  • MAX6900: FAQ
  • +MAX6900ETTAEQ-T: FAQ
  • +MAX6953EAX+: FAQ
  • +MAX713: FAQ
  • +MAX7452: FAQ
  • +MAX7456EUI+_T1: FAQ
  • MAX77650: FAQ
  • +MAX77650AEWV+: FAQ
  • +MAX77650BEWV+: FAQ
  • +MAX77650CEWV+: FAQ
  • +MAX77651AEWV+: FAQ
  • +MAX77654AENV+: FAQ
  • +MAX77654AENVN+: FAQ
  • +MAX77654BENV+: FAQ
  • +MAX77654_NV+_A1: FAQ
  • +MAX77734AENP+T: FAQ
  • +MAX77734BENP+: FAQ
  • +MAX77818 CHARGER+F: FAQ
  • +MAX77818EVKIT#: FAQ
  • +MAX77818EVSYS#: FAQ
  • MAX77818EWZ+: FAQ
  • +MAX77818EWZ+T: FAQ
  • +MAX77840EVKIT#: FAQ
  • MAX77950: FAQ
  • +MAX77950EVKIT#: FAQ
  • +MAX77950EWW+_B1: FAQ
  • +MAX77960BEFV06+: FAQ
  • MAX77961EFV+: FAQ
  • +MAX77961EFV+T: FAQ
  • +MAX77961EFV06+T: FAQ
  • +MAX77962EWJ+_B1: FAQ
  • +MAX77962EWJ12+: FAQ
  • +MAX77975EFD+: FAQ
  • +MAX77976EFD+: FAQ
  • +MAX8677AETG+: FAQ
  • +MAX8713EVKIT: FAQ
  • +MAX8856ETD+: FAQ
  • +MAX8895VEWA+: FAQ
  • +MAX8903A: FAQ
  • +MAX8934AETI+: FAQ
  • MAX8971: FAQ
  • +MAX8971CEWP+: FAQ
  • +MAX8971EWP+T: FAQ

How does the Burst mode in the MAX14745 work?

The MAX14745 Buck regulators feature a variable frequency mode for increased efficiency during light-load operation. However, there is a feature where pulse frequency modulation can be switched to peak current mode for noise sensitive applications. However, efficiency will be compromised in that mode. Please see bit 7 (Buck1LowEMI and Buck2LowEMI) of Buck1Vset and Buck2Vset registers. If you are concerned about EMI then you should use the lowEMI feature. The buck converters can output load current of up to 200mA with 900nA quiescent current.

The selection of inductors is explicitly recommended in the datasheet page 62. Device is recommended to use with 2.2uH inductor as said on page 62 Table 36 of the datasheet.

Tags: MAX14745AEWX+ emi MAX14745 burst KA-05719 buck Show More