Yes, we should follow the latest version of the datasheet – 4.7uF +10ohm from HV to DCIN. The 10 ohm resistor is required for hot plug performance. During a hot plug event the internal ESD structures of the switch pins can be forwarded biased to HV due to the fact that HV will take a longer time to stabilize. The 10 ohms is used to limit the current flow through the device in this event.