Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 2: Achieving Phase Repeatability

    This article discusses a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a...

EngineerZone
EngineerZone
Battery Management System
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Battery Management System
  • Power Management
Battery Management System
Documents How do l convert the current register value to actual current value for MAX17201, MAX17211, MAX17205, MAX17215?
  • Q&A
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADBMS6830: FAQ
  • +ADP5061: FAQ
  • +DS2438: FAQ
  • +DS2438Z+: FAQ
  • +DS2704G+: FAQ
  • +DS2711: FAQ
  • +DS2711E+: FAQ
  • +DS2712E+: FAQ
  • +DS2712EVKIT+: FAQ
  • DS2715: FAQ
  • +DS2715BZ+: FAQ
  • DS2740: FAQ
  • +DS2740U: FAQ
  • +DS2745EVKIT+: FAQ
  • +DS2745U+: FAQ
  • +DS2762AE+: FAQ
  • +DS2764AE+025: FAQ
  • DS2775: FAQ
  • +DS2775G+: FAQ
  • +DS2777: FAQ
  • +DS2781AE+/: FAQ
  • +DS2782E+: FAQ
  • DS2784: FAQ
  • +DS2784G+: FAQ
  • +DS2786: FAQ
  • DS2788: FAQ
  • DS2788E+: FAQ
  • +DS2788E+T&R: FAQ
  • +DS2788EVKIT+: FAQ
  • How do I create a model with DS2788
  • MAX14690: FAQ
  • +MAX14690AEVAL#: FAQ
  • +MAX14745AEWX+: FAQ
  • +MAX14745DEWX+: FAQ
  • +MAX14745GEWX+: FAQ
  • +MAX14745MEWX+T: FAQ
  • +MAX14920ECB+: FAQ
  • +MAX14921 EVKIT SOF: FAQ
  • MAX14921: FAQ
  • +MAX14921ECS+: FAQ
  • +MAX1501: FAQ
  • +MAX1555EZK+T: FAQ
  • +MAX16016: FAQ
  • +MAX1667EAP_T1: FAQ
  • +MAX17043G+T: FAQ
  • +MAX17043G+U: FAQ
  • +MAX17043X+: FAQ
  • MAX17048: FAQ
  • MAX17048G+: FAQ
  • +MAX17048G+CHU: FAQ
  • +MAX17049: FAQ
  • +MAX17050X+T10: FAQ
  • MAX17055: FAQ
  • MAX17055AEWL+: FAQ
  • +MAX17055AEWL+_B1: FAQ
  • MAX17055ETB+: FAQ
  • +MAX17055ETB+T: FAQ
  • +MAX17055EWL+T: FAQ
  • +MAX17055GEVKIT: FAQ
  • +MAX17058: FAQ
  • MAX17201: FAQ
  • MAX17201G+: FAQ
  • +MAX17201G+T0E: FAQ
  • MAX17201G+T: FAQ
  • +MAX17201GEVKIT#: FAQ
  • MAX17205: FAQ
  • MAX17205G+: FAQ
  • -MAX17205G+T: FAQ
    • After selecting a default Murata thermistor in the MAX17201/205/211/215 ModelGauge GUI, the Configuration wizard clears the nTGain and nTOff registers. Is this a bug?
    • Can the MAX17205 be used with more than 15 cells in series?
    • Choosing the right part for measuring 8-cell lithium iron phosphate (LiFePO4) battery
    • Could MAX17205 be supported for monitoring and balancing a 4S pack?
    • Does MAX17205 support Nickel-cadmium (NiCd) batteries or Nickel-metal-hydride (NiMH) batteries?
    • For the MAX17201/05/11/15 Fuel Gauges, what should I do with the THERM, AIN1 and AIN2 pins if I do not implement temperature monitoring?
    • How do l convert the current register value to actual current value for MAX17201, MAX17211, MAX17205, MAX17215?
    • How to achieve a proper boot sequence for the MAX17205?
    • How to achieve cell balancing for the MAX17205 in a low power application?
    • How to load a battery model without triggering an NV write cycle?
    • How to power the MAX17205 with the battery pack of more than 4 cells in series?
    • How to use memory locks in MAX1720x design?
    • In MAX17201/5 GUI how to change the cell capacity?
    • Should the I2C address of MAX17201, MAX17205 be 0001011x or 0010110x?
    • The MAX17201, MAX17211, MAX17205, MAX17215 nPackCfg Register (1B5h) is related to battery pack configuration. Should this register have the same content as PackCfg (0BDh) register?
    • The voltage, current, and temperature values read from MAX17201, MAX17205, MAX17211, MAX17215 are correct, but the RepSOC is always 1.0%. Why is that?
    • What is the MAX17205 I2C address?
    • When using the MAX17205, how do we determine if the battery is charging or discharging?
  • +MAX17205GEVKIT#: FAQ
  • +MAX17211G+: FAQ
  • +MAX17215G+: FAQ
  • +MAX17260 EVALUATION KIT SOFTWARE: FAQ
  • MAX17260BEWL+: FAQ
  • +MAX17260BEWL+_B1: FAQ
  • +MAX17260SETD+: FAQ
  • +MAX17260SEWL+: FAQ
  • +MAX17260XEVKIT#: FAQ
  • +MAX17261GEVKIT#: FAQ
  • MAX17261METD+: FAQ
  • +MAX17261METD+T: FAQ
  • +MAX17261MEWL+: FAQ
  • +MAX17261XEVKIT#: FAQ
  • +MAX17262REWL+: FAQ
  • +MAX17263GEVKIT#: FAQ
  • +MAX17263LETD+: FAQ
  • +MAX17301G+: FAQ
  • +MAX17301GEVKIT#: FAQ
  • +MAX17303G+: FAQ
  • +MAX17303X+T: FAQ
  • +MAX17313G+: FAQ
  • +MAX17320G10+: FAQ
  • +MAX17320G1EVKIT#: FAQ
  • +MAX17320G20+: FAQ
  • +MAX17320X22+: FAQ
  • +MAX17320X2EVKIT#: FAQ
  • MAX1737: FAQ
  • +MAX1737EEI+T: FAQ
  • +MAX17435: FAQ
  • +MAX1757EAI+: FAQ
  • +MAX1758EAI (28-SSOP): FAQ
  • +MAX1758EAI+: FAQ
  • +MAX17703ATG+: FAQ
  • MAX17823BGCB/V+: FAQ
  • +MAX17823BGCB/V+T: FAQ
  • +MAX17841BGUE/V+T: FAQ
  • MAX17843: FAQ
  • MAX17843ACB/V+: FAQ
  • +MAX17843ACB/V+_T1: FAQ
  • +MAX17851EVKIT#: FAQ
  • +MAX17852ACB/V+: FAQ
  • +MAX17852EVKIT#: FAQ
  • +MAX17853ACB/V+: FAQ
  • +MAX17853EVKIT#: FAQ
  • +MAX1870AETJ+: FAQ
  • +MAX1873REEE+: FAQ
  • MAX1873REEE: FAQ
  • +MAX1873TEEE+: FAQ
  • +MAX20094ATI/VY+: FAQ
  • +MAX20094ATIB/VY+: FAQ
  • MAX20303: FAQ
  • MAX20303AEWN+: FAQ
  • +MAX20303AEWN+T: FAQ
  • +MAX20303BEWN+: FAQ
  • +MAX20303EVKIT#: FAQ
  • +MAX20303EWN+: FAQ
  • +MAX20335AEWX+: FAQ
  • +MAX20353: FAQ
  • +MAX20360AEWZ+: FAQ
  • +MAX6361: FAQ
  • MAX6900: FAQ
  • +MAX6900ETTAEQ-T: FAQ
  • +MAX6953EAX+: FAQ
  • +MAX713: FAQ
  • +MAX7452: FAQ
  • +MAX7456EUI+_T1: FAQ
  • MAX77650: FAQ
  • +MAX77650AEWV+: FAQ
  • +MAX77650BEWV+: FAQ
  • +MAX77650CEWV+: FAQ
  • +MAX77651AEWV+: FAQ
  • +MAX77654AENV+: FAQ
  • +MAX77654AENVN+: FAQ
  • +MAX77654BENV+: FAQ
  • +MAX77654_NV+_A1: FAQ
  • +MAX77734AENP+T: FAQ
  • +MAX77734BENP+: FAQ
  • +MAX77818 CHARGER+F: FAQ
  • +MAX77818EVKIT#: FAQ
  • +MAX77818EVSYS#: FAQ
  • MAX77818EWZ+: FAQ
  • +MAX77818EWZ+T: FAQ
  • +MAX77840EVKIT#: FAQ
  • MAX77950: FAQ
  • +MAX77950EVKIT#: FAQ
  • +MAX77950EWW+_B1: FAQ
  • +MAX77960BEFV06+: FAQ
  • MAX77961EFV+: FAQ
  • +MAX77961EFV+T: FAQ
  • +MAX77961EFV06+T: FAQ
  • +MAX77962EWJ+_B1: FAQ
  • +MAX77962EWJ12+: FAQ
  • +MAX77975EFD+: FAQ
  • +MAX77976EFD+: FAQ
  • +MAX8677AETG+: FAQ
  • +MAX8713EVKIT: FAQ
  • +MAX8856ETD+: FAQ
  • +MAX8895VEWA+: FAQ
  • +MAX8903A: FAQ
  • +MAX8934AETI+: FAQ
  • MAX8971: FAQ
  • +MAX8971CEWP+: FAQ
  • +MAX8971EWP+T: FAQ

How do l convert the current register value to actual current value for MAX17201, MAX17211, MAX17205, MAX17215?

 
Current register format is in 2's complement. The LSB size is 1.5625uV/RSENSE, where RSENSE is the sense resistor.
 
For example,  for MAX17201evkit, the default sense resistor is 0.01ohm. Thus the LSB size would be 1.5625uV/(10mohm) = 0.15625mA
The table below is a capture from the evkit GUI as an example.

  

To convert from 0xF163 to the corresponding current, the calculation is as follow:
Since the most significant bit is high, this is a negative current.

To convert from the binary value to decimal,
0xFFFF-0xF163+1=0x0E9D=3741 in magnitude.
current = -3741*0.15625mA=-584.53125mA, which matches the value posted in the GUI above.
 

Tags: MAX17211 MAX17201 000102487 MAX17215 MAX17205G+