Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    View All Webinars
  • Community Hub

    Challenge Yourself!

      New KCC Quiz AQQ299 about Opamp Open Loop Gain and LTspice

      A kind proposal from Al Butvidas 1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
Battery Management System
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Battery Management System
  • Power Management
Battery Management System
Documents How does current sense measurement error affect fuel gauging error?
  • Q&A
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADBMS6830: FAQ
  • +ADP5061: FAQ
  • +DS2438: FAQ
  • +DS2438Z+: FAQ
  • +DS2704G+: FAQ
  • +DS2711: FAQ
  • +DS2711E+: FAQ
  • +DS2712E+: FAQ
  • +DS2712EVKIT+: FAQ
  • DS2715: FAQ
  • +DS2715BZ+: FAQ
  • DS2740: FAQ
  • +DS2740U: FAQ
  • +DS2745EVKIT+: FAQ
  • +DS2745U+: FAQ
  • +DS2762AE+: FAQ
  • +DS2764AE+025: FAQ
  • DS2775: FAQ
  • +DS2775G+: FAQ
  • +DS2777: FAQ
  • +DS2781AE+/: FAQ
  • +DS2782E+: FAQ
  • DS2784: FAQ
  • +DS2784G+: FAQ
  • +DS2786: FAQ
  • DS2788: FAQ
  • DS2788E+: FAQ
  • +DS2788E+T&R: FAQ
  • +DS2788EVKIT+: FAQ
  • How do I create a model with DS2788
  • MAX14690: FAQ
  • +MAX14690AEVAL#: FAQ
  • +MAX14745AEWX+: FAQ
  • +MAX14745DEWX+: FAQ
  • +MAX14745GEWX+: FAQ
  • +MAX14745MEWX+T: FAQ
  • +MAX14920ECB+: FAQ
  • +MAX14921 EVKIT SOF: FAQ
  • MAX14921: FAQ
  • +MAX14921ECS+: FAQ
  • +MAX1501: FAQ
  • +MAX1555EZK+T: FAQ
  • +MAX16016: FAQ
  • +MAX1667EAP_T1: FAQ
  • +MAX17043G+T: FAQ
  • +MAX17043G+U: FAQ
  • +MAX17043X+: FAQ
  • MAX17048: FAQ
  • MAX17048G+: FAQ
  • +MAX17048G+CHU: FAQ
  • +MAX17049: FAQ
  • +MAX17050X+T10: FAQ
  • MAX17055: FAQ
  • MAX17055AEWL+: FAQ
  • +MAX17055AEWL+_B1: FAQ
  • MAX17055ETB+: FAQ
  • +MAX17055ETB+T: FAQ
  • +MAX17055EWL+T: FAQ
  • +MAX17055GEVKIT: FAQ
  • +MAX17058: FAQ
  • MAX17201: FAQ
  • MAX17201G+: FAQ
  • +MAX17201G+T0E: FAQ
  • MAX17201G+T: FAQ
  • -MAX17201GEVKIT#: FAQ
    • How can I set the voltage to lower than 3.0V for battery empty, In the MAX17201EVKIT?
    • How do I select the size of my Sense Resistor for a Maxim Fuel Gauge?
    • How does current sense measurement error affect fuel gauging error?
    • How much current can the REG2 output of the MAX17201 supply? (and REG3 on MAX17211)?
    • How to prevent use of old batteries with MAX17201
    • In the MAX17201, are updates to the Secret handled separately from updates to the NVRAM?
    • In the MAX17201, why at no load state the current measurement offset error is too high and does not comply with the datasheet?
    • MAX17201 and MAX17261 configuration .ini file for primary cells
    • On a MAX17201 or other Maxim Fuel Gauge, if Config.SHDN is set to 1 to enter shutdown mode, do I need to clear Config.SHDN upon exiting shutdown mode?
    • The MAX17201GEVKIT does not go into shutdown mode after writing SHDN bit to 1, why is that?
    • Use of MAX17201 without using SHA256
    • What is the difference between fuel gauge host and pack side devices?
    • What is the difference between supply voltage and startup voltage on MAX17201
    • Where is the Vrecovery register in the MAX17201EVKIT GUI?
    • Why do I get a "Fail MTP" message on ModelGauge m5 Fuel Gauge tool when trying to program the NV memory of the MAX17201?
    • Why do Maxim fuel gauges, such as the MAX17201, have SHA-256 Secure Authentication?
  • MAX17205: FAQ
  • MAX17205G+: FAQ
  • +MAX17205G+T: FAQ
  • +MAX17205GEVKIT#: FAQ
  • +MAX17211G+: FAQ
  • +MAX17215G+: FAQ
  • +MAX17260 EVALUATION KIT SOFTWARE: FAQ
  • MAX17260BEWL+: FAQ
  • +MAX17260BEWL+_B1: FAQ
  • +MAX17260SETD+: FAQ
  • +MAX17260SEWL+: FAQ
  • +MAX17260XEVKIT#: FAQ
  • +MAX17261GEVKIT#: FAQ
  • MAX17261METD+: FAQ
  • +MAX17261METD+T: FAQ
  • +MAX17261MEWL+: FAQ
  • +MAX17261XEVKIT#: FAQ
  • +MAX17262REWL+: FAQ
  • +MAX17263GEVKIT#: FAQ
  • +MAX17263LETD+: FAQ
  • +MAX17301G+: FAQ
  • +MAX17301GEVKIT#: FAQ
  • +MAX17303G+: FAQ
  • +MAX17303X+T: FAQ
  • +MAX17313G+: FAQ
  • +MAX17320G10+: FAQ
  • +MAX17320G1EVKIT#: FAQ
  • +MAX17320G20+: FAQ
  • +MAX17320X22+: FAQ
  • +MAX17320X2EVKIT#: FAQ
  • MAX1737: FAQ
  • +MAX1737EEI+T: FAQ
  • +MAX17435: FAQ
  • +MAX1757EAI+: FAQ
  • +MAX1758EAI (28-SSOP): FAQ
  • +MAX1758EAI+: FAQ
  • +MAX17703ATG+: FAQ
  • MAX17823BGCB/V+: FAQ
  • +MAX17823BGCB/V+T: FAQ
  • +MAX17841BGUE/V+T: FAQ
  • MAX17843: FAQ
  • MAX17843ACB/V+: FAQ
  • +MAX17843ACB/V+_T1: FAQ
  • +MAX17851EVKIT#: FAQ
  • +MAX17852ACB/V+: FAQ
  • +MAX17852EVKIT#: FAQ
  • +MAX17853ACB/V+: FAQ
  • +MAX17853EVKIT#: FAQ
  • +MAX1870AETJ+: FAQ
  • +MAX1873REEE+: FAQ
  • MAX1873REEE: FAQ
  • +MAX1873TEEE+: FAQ
  • +MAX20094ATI/VY+: FAQ
  • +MAX20094ATIB/VY+: FAQ
  • MAX20303: FAQ
  • MAX20303AEWN+: FAQ
  • +MAX20303AEWN+T: FAQ
  • +MAX20303BEWN+: FAQ
  • +MAX20303EVKIT#: FAQ
  • +MAX20303EWN+: FAQ
  • +MAX20335AEWX+: FAQ
  • +MAX20353: FAQ
  • +MAX20360AEWZ+: FAQ
  • +MAX6361: FAQ
  • MAX6900: FAQ
  • +MAX6900ETTAEQ-T: FAQ
  • +MAX6953EAX+: FAQ
  • +MAX713: FAQ
  • +MAX7452: FAQ
  • +MAX7456EUI+_T1: FAQ
  • MAX77650: FAQ
  • +MAX77650AEWV+: FAQ
  • +MAX77650BEWV+: FAQ
  • +MAX77650CEWV+: FAQ
  • +MAX77651AEWV+: FAQ
  • +MAX77654AENV+: FAQ
  • +MAX77654AENVN+: FAQ
  • +MAX77654BENV+: FAQ
  • +MAX77654_NV+_A1: FAQ
  • +MAX77734AENP+T: FAQ
  • +MAX77734BENP+: FAQ
  • +MAX77818 CHARGER+F: FAQ
  • +MAX77818EVKIT#: FAQ
  • +MAX77818EVSYS#: FAQ
  • MAX77818EWZ+: FAQ
  • +MAX77818EWZ+T: FAQ
  • +MAX77840EVKIT#: FAQ
  • MAX77950: FAQ
  • +MAX77950EVKIT#: FAQ
  • +MAX77950EWW+_B1: FAQ
  • +MAX77960BEFV06+: FAQ
  • MAX77961EFV+: FAQ
  • +MAX77961EFV+T: FAQ
  • +MAX77961EFV06+T: FAQ
  • +MAX77962EWJ+_B1: FAQ
  • +MAX77962EWJ12+: FAQ
  • +MAX77975EFD+: FAQ
  • +MAX77976EFD+: FAQ
  • +MAX8677AETG+: FAQ
  • +MAX8713EVKIT: FAQ
  • +MAX8856ETD+: FAQ
  • +MAX8895VEWA+: FAQ
  • +MAX8903A: FAQ
  • +MAX8934AETI+: FAQ
  • MAX8971: FAQ
  • +MAX8971CEWP+: FAQ
  • +MAX8971EWP+T: FAQ

How does current sense measurement error affect fuel gauging error?

Hybrid coulomb-counting fuel gauges measure both battery voltage and battery current to estimate percent State-of-Charge (SOC). The effect of current sensing measurement errors on fuel gauging error depends on the type of measurement error.  As an example, measurement errors can be modeled using a formula such as:

I_measured = (1+Gain_error)*I_actual + Offset_error

As an example, take the case where Gain_error = 0.1 and Offset_error = 0; this implies a system with 10% gain error and zero offset.  The MAX17xxx family of fuel gauges report the SOC as percentage of total capacity, and one way they measure total capacity is by monitoring the total charging current it takes to move the battery from 0% charged to 100% charged.  For example, if a battery needs an actual charge of 1A for 1 hour to go from 0% to 100%, this would imply an actual capacity of 1A-hr.  A measurement Gain_error of 0.1 would make the fuel gauge measure that it took 1.1A for 1 hour to charge, so it would measure 1.1 A-hr of capacity.  However, since the discharging current would have the same gain error, it would also look like it discharged 1.1A for 1 hour to go from 100% to 0%, and also have 1.1A-hr capacity.  The 50% SOC would still happen after 30 minutes.    

For the case where Gain_error = 0, and Offset_error = 0.1A, an actual current of 0A would be measured as 0.1A.  If a 1A-hr battery was charged at 100% and had an actual current of 0A for 1 hour, the fuel gauge would measure 0.1A being discharged for 1 hour.  In this case, the fuel gauge would estimate SOC to be 90%, which would be a 10% error. The error would increase by another 10% after another hour. In actuality, the ModelGauge algorithm will bound this error because it also uses battery voltage information, but this type of offset error should be minimized by careful schematic and PCB design.  Typical causes of offset error are improper current sense resistor layout that has additional currents that do not flow into or out of the battery flowing through the sense resistor, and improper Kelvin-sensing of the current sense resistor that can appear as additional error current not actually flowing through it. 

Tags: 000097281 Battery Management System MAX17201