This webinar will introduce remote-controlled edge nodes and how they promise to simplify the automotive network architecture and expedite the integration...
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
      1. Quote of the week: "Knowledge is knowing a tomato is a fruit. Wisdom is not putting it in a fruit salad" - unknown Sources: commons.wikimedia...

    View All

    What's Brewing

      Quiz! Why a Hybrid Approach Works Blog and Test Your Knowledge

      Quiz! Understand ISO 26262 Compliance Test your knowledge with our quick quiz , based on the blog " Safety in Layers: Why a Hybrid Approach Works ...
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
    The Limitation of Heat Dissipation IO-Link is used across many branches of factory automation, and in these applications, areas of the factory floor...

     

    GMSL Debugging: Getting a Lock

    Imagine a scenario where you have a brand-new board design or are excited to try out some evaluation kits only to find out that the two devices can’t talk...
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
Battery Management System
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Battery Management System
  • Power Management
Battery Management System
Documents How do you simulate a battery for production line tests of battery chargers?
  • Q&A
  • FAQs/ Docs
  • Members
  • Tags
  • More
  • Cancel
  • +Documents
  • +ADBMS6830: FAQ
  • +ADP5061: FAQ
  • +DS2438: FAQ
  • +DS2438Z+: FAQ
  • +DS2704G+: FAQ
  • +DS2711: FAQ
  • +DS2711E+: FAQ
  • +DS2712E+: FAQ
  • +DS2712EVKIT+: FAQ
  • DS2715: FAQ
  • +DS2715BZ+: FAQ
  • DS2740: FAQ
  • +DS2740U: FAQ
  • +DS2745EVKIT+: FAQ
  • +DS2745U+: FAQ
  • +DS2762AE+: FAQ
  • +DS2764AE+025: FAQ
  • DS2775: FAQ
  • +DS2775G+: FAQ
  • +DS2777: FAQ
  • +DS2781AE+/: FAQ
  • +DS2782E+: FAQ
  • DS2784: FAQ
  • +DS2784G+: FAQ
  • +DS2786: FAQ
  • DS2788: FAQ
  • DS2788E+: FAQ
  • +DS2788E+T&R: FAQ
  • +DS2788EVKIT+: FAQ
  • How do I create a model with DS2788
  • MAX14690: FAQ
  • +MAX14690AEVAL#: FAQ
  • +MAX14745AEWX+: FAQ
  • +MAX14745DEWX+: FAQ
  • +MAX14745GEWX+: FAQ
  • +MAX14745MEWX+T: FAQ
  • +MAX14920ECB+: FAQ
  • +MAX14921 EVKIT SOF: FAQ
  • MAX14921: FAQ
  • +MAX14921ECS+: FAQ
  • +MAX1501: FAQ
  • +MAX1555EZK+T: FAQ
  • +MAX16016: FAQ
  • +MAX1667EAP_T1: FAQ
  • +MAX17043G+T: FAQ
  • +MAX17043G+U: FAQ
  • +MAX17043X+: FAQ
  • MAX17048: FAQ
  • MAX17048G+: FAQ
  • +MAX17048G+CHU: FAQ
  • +MAX17049: FAQ
  • +MAX17050X+T10: FAQ
  • MAX17055: FAQ
  • MAX17055AEWL+: FAQ
  • +MAX17055AEWL+_B1: FAQ
  • MAX17055ETB+: FAQ
  • +MAX17055ETB+T: FAQ
  • +MAX17055EWL+T: FAQ
  • +MAX17055GEVKIT: FAQ
  • +MAX17058: FAQ
  • MAX17201: FAQ
  • MAX17201G+: FAQ
  • +MAX17201G+T0E: FAQ
  • MAX17201G+T: FAQ
  • +MAX17201GEVKIT#: FAQ
  • MAX17205: FAQ
  • MAX17205G+: FAQ
  • +MAX17205G+T: FAQ
  • +MAX17205GEVKIT#: FAQ
  • +MAX17211G+: FAQ
  • +MAX17215G+: FAQ
  • +MAX17260 EVALUATION KIT SOFTWARE: FAQ
  • MAX17260BEWL+: FAQ
  • +MAX17260BEWL+_B1: FAQ
  • +MAX17260SETD+: FAQ
  • +MAX17260SEWL+: FAQ
  • +MAX17260XEVKIT#: FAQ
  • +MAX17261GEVKIT#: FAQ
  • MAX17261METD+: FAQ
  • +MAX17261METD+T: FAQ
  • +MAX17261MEWL+: FAQ
  • +MAX17261XEVKIT#: FAQ
  • +MAX17262REWL+: FAQ
  • +MAX17263GEVKIT#: FAQ
  • +MAX17263LETD+: FAQ
  • +MAX17301G+: FAQ
  • +MAX17301GEVKIT#: FAQ
  • +MAX17303G+: FAQ
  • +MAX17303X+T: FAQ
  • +MAX17313G+: FAQ
  • +MAX17320G10+: FAQ
  • +MAX17320G1EVKIT#: FAQ
  • +MAX17320G20+: FAQ
  • +MAX17320X22+: FAQ
  • +MAX17320X2EVKIT#: FAQ
  • MAX1737: FAQ
  • +MAX1737EEI+T: FAQ
  • +MAX17435: FAQ
  • +MAX1757EAI+: FAQ
  • +MAX1758EAI (28-SSOP): FAQ
  • +MAX1758EAI+: FAQ
  • +MAX17703ATG+: FAQ
  • MAX17823BGCB/V+: FAQ
  • +MAX17823BGCB/V+T: FAQ
  • +MAX17841BGUE/V+T: FAQ
  • MAX17843: FAQ
  • MAX17843ACB/V+: FAQ
  • +MAX17843ACB/V+_T1: FAQ
  • +MAX17851EVKIT#: FAQ
  • +MAX17852ACB/V+: FAQ
  • +MAX17852EVKIT#: FAQ
  • +MAX17853ACB/V+: FAQ
  • +MAX17853EVKIT#: FAQ
  • +MAX1870AETJ+: FAQ
  • +MAX1873REEE+: FAQ
  • MAX1873REEE: FAQ
  • +MAX1873TEEE+: FAQ
  • +MAX20094ATI/VY+: FAQ
  • +MAX20094ATIB/VY+: FAQ
  • MAX20303: FAQ
  • MAX20303AEWN+: FAQ
  • +MAX20303AEWN+T: FAQ
  • +MAX20303BEWN+: FAQ
  • +MAX20303EVKIT#: FAQ
  • +MAX20303EWN+: FAQ
  • +MAX20335AEWX+: FAQ
  • +MAX20353: FAQ
  • +MAX20360AEWZ+: FAQ
  • +MAX6361: FAQ
  • MAX6900: FAQ
  • +MAX6900ETTAEQ-T: FAQ
  • +MAX6953EAX+: FAQ
  • +MAX713: FAQ
  • +MAX7452: FAQ
  • +MAX7456EUI+_T1: FAQ
  • MAX77650: FAQ
  • +MAX77650AEWV+: FAQ
  • +MAX77650BEWV+: FAQ
  • +MAX77650CEWV+: FAQ
  • +MAX77651AEWV+: FAQ
  • +MAX77654AENV+: FAQ
  • +MAX77654AENVN+: FAQ
  • +MAX77654BENV+: FAQ
  • +MAX77654_NV+_A1: FAQ
  • +MAX77734AENP+T: FAQ
  • +MAX77734BENP+: FAQ
  • +MAX77818 CHARGER+F: FAQ
  • +MAX77818EVKIT#: FAQ
  • +MAX77818EVSYS#: FAQ
  • MAX77818EWZ+: FAQ
  • -MAX77818EWZ+T: FAQ
    • Battery detect in MAX77818
    • Can MAX77818 turn off internal FET between SYS and BATT pins in ship mode?
    • Can the VIO pin of MAX77818 be supplied externally?
    • Do I need to change the Lsel bit in the 0xB8 register of the MAX77818, based off of the inductor I'm using?
    • Does the MAX77818 know the capacity of a discharged battery?
    • Does the MAX77818 provide VIO?
    • How are TOFF and TGAIN selected for MAX77818?
    • How can I read out the current of the MAX77818?
    • How do you simulate a battery for production line tests of battery chargers?
    • How to avoid a POR when CHGIN is re,oved for the MAX77818?
    • How to get VSYS > 3.7V at all times even when VBAT < 3.7V for the MAX77818?
    • Is it possible to set MAX77818 Default Current Limit to 4000mA?
    • MAX77818 efficiency data in the different configurations
    • MAX77818はBattery pack側に実装するものですか、それともsystem sideに実装することを想定した製品ですか
    • On MAX77818 is it possible connect INTB through a pull up to VIO>VSYS
    • What is a workaround to quickly restore the correct SOC and RemCap when exiting standby mode without waiting for voltage fuel gauge correction on the MAX77818?
    • What is AICL mode of MAX77818?
    • What is the MAX77818 BYP pin maximum current when the device is powered only by a battery and reverse boost is adjusted to 5V?
    • What pin does the MAX77818 detect battery insertion and removal on?
    • Why am I not able to change the charge configuration settings on the MAX77818?
  • +MAX77840EVKIT#: FAQ
  • MAX77950: FAQ
  • +MAX77950EVKIT#: FAQ
  • +MAX77950EWW+_B1: FAQ
  • +MAX77960BEFV06+: FAQ
  • MAX77961EFV+: FAQ
  • +MAX77961EFV+T: FAQ
  • +MAX77961EFV06+T: FAQ
  • +MAX77962EWJ+_B1: FAQ
  • +MAX77962EWJ12+: FAQ
  • +MAX77975EFD+: FAQ
  • +MAX77976EFD+: FAQ
  • +MAX8677AETG+: FAQ
  • +MAX8713EVKIT: FAQ
  • +MAX8856ETD+: FAQ
  • +MAX8895VEWA+: FAQ
  • +MAX8903A: FAQ
  • +MAX8934AETI+: FAQ
  • MAX8971: FAQ
  • +MAX8971CEWP+: FAQ
  • +MAX8971EWP+T: FAQ

How do you simulate a battery for production line tests of battery chargers?

Much of the lab work can be done with a resistor and a lab supply.  Batteries can be used,  but when one needs to check performance at high and low voltages the resistor plus power supply is more convenient and much quicker for a production line environment. Another possibility is a lab amplifier which will source and sink current; its output voltage can be varied and it will source or sink the current sort of like a battery though the voltage is fairly constant.

The resistor needs to be a small enough value so that the max charger current flows in the resistor when testing at low voltage, and the lab supply needs to give enough current to keep the voltage across the resistor constant at high voltage. For example, if the voltage range  is 3V to 4.2V and the charge current is 3A, the resistor would be 1ohm, If the charge voltage is 4.2V, a constant current/constant voltage charger would be near 0A, so the lab supply would have to supply up to 4.2A. The lab supply voltage can be varied to simulate the range of battery voltages.
 

 
 
Tags: MAX77818EWZ+ 000097232
  • Share
  • History
  • Cancel
 
Related Content
  • RE: AD737 - negative output voltage swing?
    ADIApproved
    Sorry for the belated reply but we had some issues with the forwarding of questions from this community that have been resolved. I wanted to post an answer in the event it will help someone else with a...
  • RE: About the role of Preload of LTC1733
    Wenwei
    Hi Yuya, The 2 Ω resistor is used to sink current from the charger. Some power supply cannot sink current (no current input, just output). If the 2Ω is not connected, the LT1733 will try to output current...
  • RE: LTC4162-L minimum input voltage
    robrien_ftr
    The issue appears to be caused by my input and battery current limits. I previously set the input current limit to 0.57 A and the battery current limit to 6.4 A. This was done to allow the LTC4162 to measure...
 
Related Content
  • RE: AD737 - negative output voltage swing?
    ADIApproved
    Sorry for the belated reply but we had some issues with the forwarding of questions from this community that have been resolved. I wanted to post an answer in the event it will help someone else with a...
  • RE: About the role of Preload of LTC1733
    Wenwei
    Hi Yuya, The 2 Ω resistor is used to sink current from the charger. Some power supply cannot sink current (no current input, just output). If the 2Ω is not connected, the LT1733 will try to output current...
  • RE: LTC4162-L minimum input voltage
    robrien_ftr
    The issue appears to be caused by my input and battery current limits. I previously set the input current limit to 0.57 A and the battery current limit to 6.4 A. This was done to allow the LTC4162 to measure...