Post Go back to editing

Is the LTC681x family still a good choice?

Thread Summary

The user is seeking a 16S measurement module with active balancing, ASIL D capability, and 3mV accuracy for LiFePO4 cells. The LTC6813 is preferred but may be outdated. The ADBMS6830 is recommended for ASIL D compliance, and details are available under NDA. The user should contact the CIC team for further support on ASIL D capabilities and product details.
AI Generated Content
Category: Datasheet/Specs
Product Number: LTC6813-1

I am searching for a solution for a 16S measurement module with active balancing. Since the simplicity of using the LT8584, I would like to choose a chip with support for it. 

Our requirements are:

Minimum cell count: 8 cells LiFePO4

Maximum cell count: 16 cells

ASIL D capability without extra MCU per module

Active balancing per cell

3mV accuracy or better, since we work with LiFePO4

At least 1000V system capability

Production warranty of like 10 years

After searching for a few days, I still cannot make a strong decision. Our candidates:

name asil balancing
LTC6813 D? LT8584
ADBMS6843 D No data made public
ADBMS6837 D No data made public
ADBMS1816 No data made public 1818 has LTC8584 support?

The LTC6813 has my preference, but seems to be outdated. Since this is a new design to continue to use in the future, I do not feel comfortable choosing this chip while it may get discontinued within 2 years or so.

The ADBMS1816 seems to be the successor, but I get a huge question mark around the ASIL capabilities.

Both the 6843 and 6837 seem to be the flagships, but we need to dive into the NDA trajectory to see if they are what we want. The 6843 is really interesting with the impedance measurement capabilities.

Can someone suggest if the LTC6813 complies with our needs? Or if it is highly recommended to choose one of the other chips. And not less important, if the LT8584 circuit will pass the ASIL D with ease.

I hope to hear from you.

Kind regards,

Robert Jan

Edit Notes

Clarification
[edited by: RobertJan at 7:42 AM (GMT -4) on 26 Jun 2026]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.