Post Go back to editing

RSENSE Value

Category: Hardware
Product Number: MAX17260

The front page of the datasheet lists the RSENSE range as 1mΩ to 1Ω. However, Table table shows that a value of up to 15.99976Ω can be programmed in. Does this mean I can actually use a 10Ω resistor so that I could get sub-microamp accuracy? I need the fuel gauge to be able to measure battery load currents that fluctuate from 1uA to 12uA most of the time, but sometimes can get as high as 100mA. 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.