Post Go back to editing

Datasheet discrepancies regarding endian-ness

Thread Summary

The user encountered discrepancies in the LTC2949 datasheet regarding byte ordering, particularly with PEC being reversed and incorrect little-endian descriptions. The final answer confirms that the LTC2949 and other ADBMS parts using isoSPI are big endian, and recommends transitioning to the ADBMS2950B for easier firmware development and better performance. The ADBMS2950B is more accurate, updates measurements faster, and has an automotive variant certified for ASIL-D.
AI Generated Content
Category: Datasheet/Specs
Product Number: LTC2949

Hi,

I am working on a project implementing the LTC2949. I've noticed a number of discrepancies in the datasheet specifically regarding byte ordering:

ltc2949.pdf, Rev A:

1. PEC appears reversed

(Page 33, table 11): For each of the frame layout tables in the datasheet, such as this one, the PEC appears with the lowest byte first in the order, followed by the highest byte. The only way to get the LTC2949 to respond to a DCMD read is with the PEC reversed so that it is represented as big endian. This is further confused by the unlabeled table on page 31 showing example transactions with the LTC2949. In the example for CONT0 at least, the PEC is actually shown as big endian. I think it must be the case that the chip is actually designed to transact PEC as big endian. I am computing PEC via the given example code on page 40.

2. Little endian blurb is wrong

(Page 42, "MEMORY MAP AND PAGING MECHANISM") Has the following blurb:

Multiple-byte data is stored with most significant byte at the lowest address (little-endian). For instance, the MSB C1[47:40] of the quantity C1 is stored at address 0x00 in PAGE0.

This blurb is incorrect. Little endian is the opposite of this statement. This is further confused by the following statement:

Note that reading data from LTC2949's memory map (no matter if using direct command or indirect memory access RDCV command with RDCVCONF=0) reports MSBytes first,

So if reading data out, do we really get the least significant byte or the actual value first since it's stored as big endian?

Would it be possible for an LT engineer to review/fix this datasheet? These are fundamental problems that make implementing this part a lot more frustrating than it should ever be.

Parents
  • Thanks for pointing out this error, LTC2949 and all other ADBMS parts which use isoSPI are indeed big endian.  The use of 'little endian" there is an error.

    At this point in LTC2949 lifecycle it is too late to make datasheet changes, as the part is in the process of being transitioned to NRND.  LTC2949 is a particularly difficult part to write firmware for due to having many significant constraints in both how many simultaneous functions it can run as well as in the timing.  ADBMS2950B is more accurate, updates its standard current sense measurements 100x faster, lower cost, and most importantly far easier to write firmware for.  It also has an automotive variant available which is certified for ASIL-D.  Unlike LTC2949, ADBMS2950B uses an internal architecture similar to the LTC68xx cell monitors with separate command codes for each read, write, and action to control the functionality.  Even if there is already prototype hardware started, we strongly recommend transitioning to ADBMS2950B as LTC2949 firmware is notoriously difficult and slow to write.

Reply
  • Thanks for pointing out this error, LTC2949 and all other ADBMS parts which use isoSPI are indeed big endian.  The use of 'little endian" there is an error.

    At this point in LTC2949 lifecycle it is too late to make datasheet changes, as the part is in the process of being transitioned to NRND.  LTC2949 is a particularly difficult part to write firmware for due to having many significant constraints in both how many simultaneous functions it can run as well as in the timing.  ADBMS2950B is more accurate, updates its standard current sense measurements 100x faster, lower cost, and most importantly far easier to write firmware for.  It also has an automotive variant available which is certified for ASIL-D.  Unlike LTC2949, ADBMS2950B uses an internal architecture similar to the LTC68xx cell monitors with separate command codes for each read, write, and action to control the functionality.  Even if there is already prototype hardware started, we strongly recommend transitioning to ADBMS2950B as LTC2949 firmware is notoriously difficult and slow to write.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.