Hello,
We are currently redesigning our ADBMS6830B-based BMS for a Formula Student EV, and I would like to ask for clarification about the clamp network used in the EVAL-ADBMS6830BMSW schematic:

I have reviewed the ADBMS6830B datasheet and the evaluation board schematic, but I still do not fully understand the purpose and design criteria of the external clamp components, especially the BAV70 devices and the SMBJ75A-13.
My main questions are the following:
- External clamp usage
In the ADBMS6830B datasheet I do not see an explicit requirement to use external clamp devices such as BAV70 or SMBJ75A-13 on the S pins or balancing network.
The datasheet mentions that the IC is hot plug tolerant without external protection, and it also shows internal protection structures in the internal protection section.
Because of this, I am not sure in which situations these external clamp components are actually required, recommended, or optional. - Why are these clamp components only used from around Cell 7 upward in the evaluation board
In the EVAL-ADBMS6830BMSW schematic, the BAV70 clamp network appears only on the upper channels, and there is also an SMBJ75A-13 on the clamp rail.
I do not understand why this is only implemented from approximately Cell 7 and above, instead of on every balancing channel.
Is this related to the absolute voltage potential of the upper cells with respect to V minus?
In other words, is the reason that from Cell 7 upward the common-mode voltage becomes high enough that additional external clamping is useful or necessary, while for the lower cells it is not?
- Can these parts be replaced by other devices
I have seen comments on the forum suggesting that these devices may be replaceable with other components, but I would like to understand the actual design target first:
Are these parts intended mainly for ESD, transient suppression, hot-plug stress, balancing switch protection, or some other specific condition? - Use with external passive balancing MOSFETs
For our design, we are implementing passive balancing with external N-channel MOSFETs, following the concept shown in Figure 40 of the datasheet.
Because I did not fully understand the reason for placing the clamp only on the upper channels in the eval board, I initially added the clamp network on every SxP and SxN pair in our redesign.
I would like to know whether this makes sense, or whether it may introduce unnecessary leakage, distortion, or other side effects in the measurement and balancing paths.

- Difference between datasheet figures and eval board values
I also noticed that the component values used in the eval board differ significantly from the values shown in the datasheet figures:
- In the functional block diagram, the balancing-related resistors are shown as 10 ohm and the capacitor as 100 nF.
- In the evaluation board schematic, I see 15 ohm resistors and 0.22 uF capacitors in the balancing-related path.
I understand that the functional block diagram is not necessarily intended as a design-ready application schematic, but I would still appreciate clarification on the practical design guidance here.
- Figure 40 issue
I have already seen another forum post indicating that Figure 40 in the datasheet contains an error, because the 10 nF capacitor is drawn from V minus to S1N, while it should actually be connected to C1.
We have already taken this into account in our redesign.

Since ADI is one of our sponsors, we would like to document this topic properly and avoid any major design mistake before finalizing the new board.
If useful, we can also share our updated schematic by email for review.
Thank you very much in advance for any clarification.
Best regards,