I encountered an issue while using the LT8490. In my application, the input voltage sometimes reaches 150V, which exceeds the chip's operating range of 0–80V. Is there any hardware solution that allows 150V to be directly or indirectly input into the LT8490 while maintaining normal operation without significantly reducing efficiency?