Post Go back to editing

Discharge/Charge Current Monitoring

Thread Summary

The user inquires about monitoring charge/discharge current and setting max/min values for shutdown using the ADBMS2950 and ADBMS6830 with BMS_BROWSER_GUI_BM. The final answer indicates that support for NDA-covered products like the ADBMS2950 is not available on EngineerZone and directs the user to contact the CIC team for assistance.
AI Generated Content
Category: Software
Product Number: ADBMS2950
Software Version: BMS_BROWSER_GUI_BM

I am using an ADBMS2950 along with two ADBMS6830 in a daisy chain to monitor a 17-cell battery pack the boards are connected to SDP-K1 through isoSPI connections. I am using BMS_BROWSER_GUI_BM to monitor and look at the cell voltages and more. I know the ADBMS2950 is capable or measuring the charge/discharge current through the shunt connected to its board. However, I can't find where on the GUI I can monitor where it is. Does anyone know if the GUI has the capabilities to measure the charge and discharge current and also set certain max or min values that will make it shut off so it doesn't hurt the system? If so, where do I find it and how would I go about setting it up?

  • A Non-Disclosure Agreement covers the product you are seeking support on, and we are unable to provide support for it in the public EngineerZone community.  Per the Analog Devices EngineerZone Code of Conduct, we do not discuss NDA products on EngineerZone.  To receive support on this product, please contact the CIC team. 

    • In the US: 800-262-5643 or 781-937-1428
    • In Europe: Contact the Customer Interaction Center (CIC), Telephone: 00800 266 822 82 or +49 89 769 03111
    • In China: Contact the Customer Interaction Center (CIC): 400-6100-006, Rest of World: ALL 01 1 781 937 1428

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.