Post Go back to editing

Issues with the MAX17320G20+ and a 4S battery pack.

Thread Summary

The user experienced issues with the MAX17320G20+ BMS IC, including IC failure and short circuits. The problem was resolved by replacing the 50 Ohm resistor on the IN pin with a 10 Ohm resistor, as recommended in the datasheet. Reg2 and Reg3 are for internal use only and should not be connected to external loads.
AI Generated Content
Category: Hardware
Product Number: MAX17320G20+, MAX17320

Good day,

I have designed a PCB that uses the MAX17320G20+ IC as the BMS for a 4S battery pack. I am having trouble with using the IC.

Note, for all initial tests I used a power supply set to 15V with 4 resistors in series to simulate the independent cells. The first IC was fine when I applied power. Then after jump starting the IC, connecting pack+ to batt, The IC powered up fine and reg3 was outputting 3.4V. I had a ADUM1252ASA+ connected to logic shift the I2C to my MCU, and after a while trying to communicate with the IC, it just suddenly let out some smoke. Reg3 was shorted to ground and the IC was dead. I figured it was because the ADUM1252ASA+ was drawing too much current from the reg3 pin. So I removed it and replace the BMS. I connected the I2C lines directly to the BMS.

This time the IC worked fine and I was able to power it up, connect batteries and all was dandy!

So I decided to do the same for the rest of my PCBs. The first one just immediately blew when trying to jump start it (Reg3 shorted to ground), so I thought it was either soldered incorrectly or it was a faulty IC. I replaced it again and this time it was fine when applying power and jump starting it. But after a while the power supply just tripped and was showing a short circuit, so I measured the resistance between the pins. The resistance between GND and batt and GND and vcell3 is very low, like 30 ohm, so I dont know what went wrong. This time Reg3 was not shorted to ground.

Please find my schematic attached. I look forward to hearing back from you.

Kind regards,

Russouw Grobbelaar

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.