Post Go back to editing

LiSoCl2 Battery Pack state of charge

Category: Hardware
Product Number: MAX17201

Hi,

I have a custom device that will use a 3 in parallel LiSoCl2 (3.6 volts) with a capacity of 39 Ah. I will need to periodically report the state of the battery and these batteries have a flat discharge curve. So I start investigating possible solutions for this and came across the MAX17201. And I have the following questions:

  • Is the MAX17201 suitable for this setup ? Or do you have any other recommendation for this setup ?
  • How this product competes with the BQ35100, since it was one of the suggestions the appeared while searching. 

Hope you can help me!

Thank you!

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.