Post Go back to editing

Initialisation for LiFePO4

Category: Software
Product Number: MAX17260

Hi,

we have chosen the max17260 for our hardware design including a charger device and a 18650 LiFePO4 battery, allowing the system to run from 5V/USB-C (whilst charging) or from a battery.

Communication to the MAX17260 works well, battery voltage and current readings are ok and plausible - during charging mode as well as battery mode. 

However, the results of the REPCAP, REPSOC, TTE and TTF readings are not making sense.

Our battery is a 1800mA LiFePO4, Vempty = 2.45V, Vcharge = 3.55V. Rsense = 10mOhm

After a POR or a software reset, the first reading appears to be mostly ok, e.g. for a fully charged battery in battery mode, it gives REPSOC 98%, REPCAP 1770mAh. TTE is not good though, i.e. 40min. 

The next readings are, however, bad, jumping down to REPSOC 4%, REPCAP 88mAh and TTE 22min. The values do change over time, but still make no sense.  

Initialisation is currently done according to EZ Config (following AppNote UG6595).

Everything I have tried, e.g. giving it time to charge or to run in battery mode, issuing a quick start, software reset, does not show improvement. 

I assume the problem could lie within the initialisation and the calculations of the m5 algorithm. Is it actually possible to get the EZ Config to work properly with a LiFePO4? 

We do not need the highest accuracy, but the values should be roughly ok and plausible.

Can anyone help? Is a custom config the only solution?

Is there a way to create our own custom config/initialisation or does anyone have a LiFePO4 config to share?

Grateful for any advice and feedback.

 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.