I have a question.
I designed a BMS board with MAX17841B+MAX17852.
Do I need to use an isolator? It works fine.
MAX17841B
Production
The MAX17841B ASCI combines an SPI port with a universal asynchronous receiver transmitter (UART) specially designed to interface with Maxim battery management...
Datasheet
MAX17841B on Analog.com
MAX17852
Production
The MAX17852 is a flexible data-acquisition system for
the management of high-voltage and low-voltage battery
modules. The system can measure 14 cell voltages...
Datasheet
MAX17852 on Analog.com



I have a question.
I designed a BMS board with MAX17841B+MAX17852.
Do I need to use an isolator? It works fine.
Hi Sunghyun,
It depends of the voltage between the chassis and the top cell: if >60V you need an isolator to avoid isolation break between MAX17841b and MAX17852.
If <60V and negative pole of cells stack is linked to chassis, only add a fuse to avoid short-circuit in case the MAX17852 is failing short.
I hope this hint helped a bit,
BegR